3.8.3 Motion Surveillance Application on SAM E54 Curiosity Ultra Development Board
Description
The Motion Surveillance application detects a motion in front of the ArduCAM (camera) using the PIR Click (motion sensor) board. ArduCAM captures an image with resolution 320x240 and stores the image in an external storage device (microSD Card). Additionally, the application demonstrates a live preview of captured images.
The live preview of captured images is demonstrated by running an HTTP web server on the development board. The user connects to the webserver through an internet browser and view the live preview of the captured images.
Modules/Technology Used
- Peripheral Modules:
- NVMCTRL
- PORT
- SYSTICK
- SERCOM - USART
- SERCOM - I2C
- SERCOM - SPI
- RTC
- SDHC
- TC
- CRYPTO
- NVIC
- System Services:
- Debug
- Command
- File System
- Time
- Console
- DMA
- Middleware libraries:
- TCP/IP Stack
- Harmony Core
- FreeRTOS
Hardware Used
- SAM E54 Curiosity Ultra Development Board v2
- Arducam Mini 2MP Plus – OV2640 SPI Camera Module
- mikroBUS Xplained Pro
- MikroElektronika PIR Click
- microSD Card
-
Note: The link above points to LAN8720A PHY Daughter Board.
The user can procure the PIC32MZ Embedded Connectivity with FPU (EF) Starter Kit and remove the LAN8740 PHY Daughter board on it and use it for this demo.
Software/Tools Used
This project has been verified to work with the following versions of software tools:
Refer Project Manifest present in harmony-manifest-success.yml under the project folder firmware/src/config/sam_e54_cult_freertos.
- Refer the Release Notes to know the MPLAB X IDE and MCC/MCC Plugin version.
- MPLAB XC32 C/C++ Compiler v2.50.
- Any Serial Terminal application, such as Tera Term terminal application.
Because Microchip regularly updates tools, occasionally issue(s) could be discovered while using the newer versions of the tools. If the project does not seem to work and version incompatibility is suspected. It is recommended to double-check and use the same versions that the project was tested with. To download original version of MPLAB Harmony v3 packages, refer to document How to Use the MPLAB Harmony v3 Project Manifest Feature (DS90003305).
Hardware Setup
- Mount the MikroElektronika PIR Click on to the mikroBUS Xplained Pro adapter and then connect the mikroBUS Xplained Pro to EXT1 of the SAM E54 Curiosity Ultra Development Board.
- Bend the VCC pin of Arducam Mini 2MP Plus – OV2640 SPI Camera
Module as shown in the following image.
- Mount the modified Arducam Mini 2MP Plus – OV2640 SPI Camera
Module on to the Arduino R3 Uno compatible interface (J503) present on the
SAM E54 Curiosity Ultra Development Board v2 and connect the
ArduCAM pins to the SAM E54 Curiosity Ultra Development Board v2 as shown bellow.
- VCC -> 3V3 pin (3.3V) of Arduino R3 Uno compatible interface using a Male to Female Jumper Wire.
- Connect the remaining ArduCAM
pins directly to the Arduino R3 Uno compatible interface (J503). For example:
- SCL -> PD08
- SDA -> PD09
- GND -> GND
- SCK -> PB25
- MISO -> PC25
- MOSI -> PB24
- CS -> PB28
- Mount LAN8740 PHY daughter board on Ethernet PHY header.
TCP/IP Network Setup

- The application is configured and build with LAN8740 PHY driver. To use a different PHY, use MPLAB Code Configurator (MCC) to select and configure the PHY. Make sure that correct PHY address and configuration flags are used for the particular PHY daughter board. The MII/RMII and I/O configuration flags should match the hardware for the PHY board. This application demonstration assumes that IPv4 is enabled. If IPv4 is not enabled in MCC, the code in app.c will not build and needs to be updated to remove the IPv4 dependencies.
- The demo has DHCP enabled, and expect a DHCP server to be available. If there is no DHCP server, then the default static IP address will be used: 192.168.100.11. If this static address does not match the network settings, use MPLAB Code Configurator (MCC) to modify the static IP address of the network interface.
- The NetBIOS name of the application is specified during the initialization of TCP/IP stack. It is the hostName member of TCPIP_HOSTS_CONFIGURATION structure. The NetBIOS service must be enabled in demonstration configuration, for the demonstration to respond to NetBIOS queries. Alternatively, use the IPv4 or IPv6 address (if IPv6 is enabled) of the board directly.
- The IPv4 and IPv6 addresses can be obtained by running the TCP/IP Discovery utility on the computer. Ex: ipconfig
Programming Hex File
The pre-built hex file can be programmed by following the below steps.
- Open MPLAB X IDE.
- Close all existing projects in IDE, if any project is opened.
- Go to File -> Import -> Hex/ELF File.
- In the Import Image File
window,
- Create Prebuilt Project,
- Click the Browse button to select the prebuilt hex file.
- Select Device as ATSAME54P20A.
- Ensure the proper tool is selected under Hardware Tool and click on Next button.
- Select Project Name and Folder,
- Select appropriate project name and folder and click on Finish button
- Create Prebuilt Project,
- In MPLAB X IDE, click on Make and Program Device button to program the device.
- Follow the steps in Running the Demo section below.
Programming/Debugging Application Project
- Open the project (same54c_motion_surveillance/firmware/sam_e54_cult_freertos.X) in MPLAB X IDE
- Ensure SAM E54 Curiosity Ultra is selected as hardware tool to program/debug the application
- Build the code and program the device by clicking on the Make and Program Device button in MPLAB X IDE tool bar
- Follow the steps in Running the Demo section below
Running the Surveillance Application Demo
- Perform Hardware Setup steps mentioned above, if not done already.
- Ensure a microSD Card is formatted and loaded with the web_pages provided within the same54c_motion_surveillance/firmware/src/web_pages directory.
- Insert this microSD Card at J704 socket (back side of the board) on SAM E54 Curiosity Ultra Development Board v2.
- Build and download the demonstration project on the target board.
- Serial Terminal
Configuration:
- Open a standard terminal application on the computer (such as Hyper-terminal or Tera Term) and configure the virtual COM port.
- Set the serial baud rate to 115200 baud in the terminal application.
- See that the initialization prints
on the serial port terminal.

- When the DHCP client is enabled in the demonstration, wait for the DHCP server to
assign an IP address for the development board. This will be printed on the serial
port terminal.

- Alternatively, use ipconfig to get the IP address of the board and ping to test if the device is reachable.
- An LED "LED2" on the SAM E54 Curiosity Ultra Development Board v2 toggles when a motion is detected in front of the motion sensor (PIR click).
- An JPEG format image with 320x240 resolution is captured and stored on the microSD Card. Check the logs in the terminal for the motion detection, start capture and saved image events.
- Steps to preview the captured
images:
- Step 1: Live streaming of
captured images:
- An HTTP server is hosted by the demonstration application. Open a web browser and direct it to the board running the HTTP server by typing the URL in the address bar (for example, https://mchpboard_c or by entering the assigned IP address i.e. http://192.168.100.11/ in the URL bar), and then press Enter key.
- On the loaded page, go to the Motion Surveillance under the left Menu.
- The following image shows how
the Motion Surveillance page looks. When the motion sensor detects a
motion, the captured images will be live previewed on this page.Note:
- When the motion sensor detects a motion, the ArduCAM captures an image (resolution 320x240) and stores in web_pages/arducam folder on the microSD Card.
- The maximum number of
images that the application stores on the microSD Card is 255. If
the number of images captured exceeds 255, the application
overwrites the images from the beginning. User can increase the storage
size based on the available free size of the microSD Card by changing the
MAX_FILE_NAMES macro in the app_ardu_cam.h header
file.
- If any error (check logs in the terminal), reset the device or reload the page or click Motion Surveillance menu option.
- Step 2: Preview the images
stored on the microSD Card using Windows Photo Viewer application:
- Remove the microSD Card from the J704 socket (back side of the board) on SAM E54 Curiosity Ultra Development Board v2 and insert into personal computer.
- Go to web_pages/arducam folder and preview the captured images using any photo preview application.
- Step 1: Live streaming of
captured images:
Comments
- Reference Training Module:
- This application demo builds and
works out of box by following the instructions above in Running the Demo
section. If the user needs to enhance/customize this application demo, should use the
MPLAB Harmony v3 Software framework. Refer links below to setup and build the
applications using MPLAB Harmony.
- How to Setup MPLAB Harmony v3 Software Development Framework (DS90003232).
- How to Build an Application by Adding a New PLIB, Driver, or Middleware to an Existing MPLAB Harmony v3 Project (DS90003253).
- MPLAB Harmony v3 is configurable through MPLAB Code Configurator (MCC). Refer to the below links for specific instructions to use MPLAB Harmony v3 with MCC.