3.7.1 Barcode Scanner Application using SAM E51 Integrated Graphics and Touch (IGAT) Curiosity Evaluation Kit
Description
This application detects the EAN-13 barcode and decodes it with the help of the ArduCAM Mega camera module. The ArduCAM Mega captures an image with a resolution of 1920x1080 and stores the image in an internal memory. The decoded barcode is then displayed on the serial console and graphical display.
Modules/Technology Used
- Peripheral Modules:
- ADC
- NVMCTRL
- EVSYS
- NVIC
- PORT
- SYSTICK
- SERCOM - SPI
- SERCOM - UART
- TC
- CCL
-
Drivers:
- SPI Driver
- External Display Controller Driver
-
System Services:
- Time
- STDIO
- Input System
-
Middleware libraries:
- Harmony Core
- Legato Graphics
Hardware Used
Software/Tools Used
This project has been verified to work with the following versions of software tools:
Refer Project Manifest present in harmony-manifest-success.yml under the project folder firmware/src/config/sam_e51_igat.
- Refer the Release Notes to know the MPLAB X IDE and MCC Plugin version.
- Any Serial Terminal application, such as Tera Term terminal application.
Because Microchip regularly updates tools, occasionally issue(s) could be discovered while using the newer versions of the tools. If the project does not seem to work and version incompatibility is suspected. It is recommended to double-check and use the same versions that the project was tested with. To download original version of MPLAB Harmony v3 packages, refer to document How to Use the MPLAB Harmony v3 Project Manifest Feature (DS90003305).
Setup
- Connect the ArduCAM Camera module to
the SAM E51 Integrated Graphics and Touch (IGAT) Curiosity Evaluation Kit as
shown below.
- Connect the ArduCAM pins directly to
the Extra Port pins interface (J203).


- Connect a micro-USB cable to the
DEBUG USB port of the SAM E51 Integrated Graphics and Touch (IGAT)
Curiosity Evaluation Kit to power the board and for programming and
debugging.
Programming Hex File
The pre-built hex file can be programmed by following the below steps.
- Open MPLAB X IDE.
- Close all existing projects in IDE, if any project is opened.
- Go to File -> Import -> Hex/ELF File.
- In the Import Image File
window,
- Create Prebuilt Project,
- Click the Browse button to select the prebuilt hex file.
- Select Device as ATSAME51J20A.
- Ensure the proper tool is selected under Hardware Tool and click on Next button.
- Select Project Name and Folder,
- Select appropriate project name and folder and click on Finish button
- Create Prebuilt Project,
- In MPLAB X IDE, click on Make and Program Device button to program the device.
- Follow the steps in Running the Demo section below.
Programming/Debugging Application Project
- Open the project (same51_barcode_scanner/firmware/sam_e51_igat.X) in MPLAB X IDE
- Ensure SAM E51 Integrated Graphics and Touch Curiosity is selected as hardware tool to program/debug the application
- Build the code and program the device by clicking on the Make and Program Device button in MPLAB X IDE tool bar
- Debugging the project can be done by clicking on the Debug Main Project button in MPLAB X IDE tool bar
- Follow the steps in Running the Demo section below
Running the Demo
- Open a standard terminal application on the computer (such as Putty or Tera Term) and configure the virtual COM port.
- Set the serial baud rate to 115200 baud in the terminal application.
- Wait for the initialization prints in the serial port terminal. If it does not show any prints, give the command “0” through terminal console which resets the development board.
- When the ArduCAM Mega Camera is enabled in the demonstration, wait for the initialization confirmation from the development board. This will be printed on the serial port terminal.
- Show the Barcode in front of the camera for capture (maintain a minimum distance of 10 to 15 cm).
- Give the command “1” through
terminal console.
- An LED “LED0” on the SAM E51 Integrated Graphics and Touch (IGAT) Curiosity Evaluation Kit toggles when the scanning is in progress.
- Once the scanning is completed, the
result will be displayed in the terminal console as well as graphical display.
Figure 3-98. Output
Note:- This demo supports EAN-13 barcodes only.
- Print the EAN-13 type barcode on a A4 sheet and show it before the ArduCAM Mega Camera module (keep a distance of 10 to 15 cm).
Comments
- Reference Applications:
- This application demo builds and
works out of box by following the instructions above in Running the Demo
section. If the user needs to enhance/customize this application demo, should use the
MPLAB Harmony v3 Software framework. Refer links below to setup and build the
applications using MPLAB Harmony.
- How to Setup MPLAB Harmony v3 Software Development Framework (DS90003232).
- How to Build an Application by Adding a New PLIB, Driver, or Middleware to an Existing MPLAB Harmony v3 Project (DS90003253).
- How to Set up the Tools Required to Get Started with MPLAB® Harmony v3 and MCC
- Create a new MPLAB Harmony v3 project using MCC
- Update and Configure an Existing MHC-based MPLAB Harmony v3 Project to MCC-based Project