3.5.3.1 Build MPLAB Harmony v3 Project with Arm GCC Toolchain in MPLAB X IDE
This page describes steps to build an MPLAB Harmony v3 project with Arm GNU Toolchain in MPLAB X IDE. The page demonstrates configuring, building, and running an MPLAB Harmony v3 peripheral library (PLIB) application with the Arm GCC toolchain developed on the SAM D21 Xplained Pro Evaluation Kit.
The application demonstrates how to use the AC (Analog Comparators) Peripheral library to perform a single-shot conversion when the peripheral is triggered by the RTC (Real-Time Counter) compare event. The generation of a trigger and compare operation is done while the CPU is in the standby sleep mode. The AC generates the interrupt at the end of the comparison which wakes the CPU.
The SAM D21 Xplained Pro Evaluation Kit is ideal for evaluating and prototyping with the SAM D21 Arm Cortex-M0+ based microcontrollers. Xplained Pro Extension kits compatible with SAM D21 Xplained Pro can be purchased individually.
MPLAB® Harmony v3 is a flexible, fully integrated embedded software development framework for 32-bit microcontrollers (MCUs) and microprocessors (MPUs). MPLAB Harmony v3 includes the MPLAB Code Configurator (MCC) tool, a set of modular Peripheral Libraries (PLIBs), drivers, system services, middleware, and numerous example applications, all of which are designed to help quickly and easily develop powerful and efficient embedded software for Microchip’s 32-bit PIC® and SAM devices.
Prerequisites
- Make sure MPLAB X IDE is installed and Harmony v3 repositories are cloned. For detailed information, refer to MPLAB® Harmony v3
- Download and install Arm GNU Toolchain v6.3.1
- Use the solution project as
an example:
- Build the solution project and program it to the SAM D21 Xplained Pro Evaluation Kit to observe the expected behavior.
- Create the project from
scratch:
- Follow step-by-step instructions below.
Instructions to Configure, Build and Run MPLAB Harmony v3 Project with Arm GCC Toolchain in MPLAB X IDE
The following bullet points provides links to the topics:
- Hardware Used
- Software/Tools Used
- Description
- Overview
- Open Project and Compile using XC32 Toolchain
- Configure the project to use Arm GCC Toolchain
- Compile the project using Arm GCC Toolchain
- Running the Demo
- Results
- Conclusions
Hardware Used
Software/Tools Used
This project has been verified to work with the following versions of software tools:
- MPLAB Harmony v3 "csp" repo v3.18.5
- MPLAB Harmony v3 "csp_apps_sam_d21_da1" repo v3.4.0
- MPLAB Code Configurator Plugin v5.5.1
- MPLAB X IDE v6.20
- Arm GNU Toolchain v6.3.1
- MPLAB XC32 Compiler v4.40
- Any Serial Terminal application, such as Tera Term terminal application.
Because Microchip regularly update tools, occasionally issue(s) could be discovered while using the newer versions of the tools. If the project does not seem to work and version incompatibility is suspected, it is recommended to double-check and use the same versions that the project was tested with.
Setting up SAM D21 Xplained Pro Evaluation Kit
- Connect a voltage below VDD to pin 17 of the EXT1 connector.
- Connect the Debug USB port on the board to the computer using a micro USB cable.
Description
Overview:
The AC Sleepwalking Harmony v3 Application on SAM D21 Xplained Pro Evaluation Kit is used to show the steps to compile the project with Arm GCC Toolchain in MPLAB X IDE.
Open Project and Compile using XC32 Toolchain:
- Open MPLAB X IDE and close if any projects are opened.
- Download the Harmony 3 peripheral library application examples for SAM D21/DA1 family csp_apps_sam_d21_da1 then go to /apps/ac/ac_sleepwalk_singleshot/firmware and select the “sam_d21_xpro.X” configuration.
- Before changing the toolchain to Arm GCC, ensure the example application demo is compiling and working fine with existing the XC32 toolchain. This is to avoid any errors because of missing library or source files.
- Select the project, right-click on it and choose Set Configuration -> Customize and go to Project Properties to ensure the correct hardware and XC32 compiler version are selected.
- Compile the project.
- Run on hardware to ensure the project is working as expected.
Configure the Project to use Arm GCC Toolchain:
This can be done with two methods, either automatically or manually.
- Automatic Detection: If
Atmel Studio is installed in PC, by default, MPLAB X IDE detects the Arm GCC
toolchain (installed as a part of Atmel Studio) and shows it in the MPLAB X
IDE's Project properties. Refer the figure which shows Arm GCC Toolchain
selection.
Since the Arm GCC toolchain is already available, switch to the Arm GCC toolchain from the project properties.
- Manual: If Atmel Studio is
not installed, install the Arm GCC toolchain manually. Go to MPLAB X IDE
-> Tools -> Options -> Embedded -> Build Tools -> Add ->
give the base directory ->
<toolchain_path>/toolchain/arm/arm-gnu-toolchain/bin". Save
it.
- Select the Arm GCC
toolchain in the example application demo project properties. Select and
right click the Project then choose Set Configuration ->
Customize and go to Project Properties. Select the Arm
GCC toolchain in compiler options and save.
- Select the Arm GCC
toolchain in the example application demo project properties. Select and
right click the Project then choose Set Configuration ->
Customize and go to Project Properties. Select the Arm
GCC toolchain in compiler options and save.
Compile the Project using Arm GCC Toolchain:
If the project is compiled at this point, the compiler may throw some errors. To avoid compiler errors, follow the below steps.
- Add include directories as shown
in the following image to avoid missing file errors for device.h and
device_cache.h.
- The include directory
paths are shown below:
- csp_apps_sam_d21_da1/apps/ac/ac_sleepwalk_singleshot/firmware/src/config/sam_d21_xpro
- csp_apps_sam_d21_da1/apps/ac/ac_sleepwalk_singleshot/firmware/src/packs/ATSAMD21J18A_DFP
- The include directory
paths are shown below:
- Comment the user row
configuration bits #pragmas from the "initialization.c" file. This
is because #pragmas are not recognized by the Arm GCC compiler.
- Add or Edit the below files to
make the project work with Arm GCC toolchain.
- Add custom Linker file to the project.
- Replace XC32 startup code with Arm GCC startup code. This can be done by adding "startup_gcc.c" file and excluding (or removing) "startup_xc32.c" file from project. Edit "libc_syscalls.c" file to compile with Arm GCC toolchain.
- Add STDIO ->
"gcc_monitor.c" file to make printf/scanf work properly.
Exclude (or remove) the "xc32_monitor.c" file from the MPLAB
Harmony v3 project.
- This can be done as follows:
- Go to config folder of Harmony v3 project config folder
- Download the SAM D21 AC Sleepwalking solution project -> samd21_ac_sleepwalk_singleshot_gcc.zip
- After downloading
the solution project, copy the files from
/apps/sam_d21_xpro/samd21_ac_sleepwalk_singleshot_gcc/src_gcc_toolchainand paste in the example application (downloaded from csp_apps_sam_d21_da1) folderapps/ac/ac_sleepwalk_singleshot/firmware/src/config/sam_d21_xpro - Paste the files "ATSAMD21J18A.ld", "startup_gcc.c" in "sam_d21_xpro" folder and "gcc_monitor.c" file in "stdio" folder.
- Right click
Linker Files in MPLABX project -> click Add
Existing Item -> select corresponding recently added
linker file and add to project. Below image is for
reference.
- Similarly, add "startup_gcc.c" file and "gcc_monitor.c" file to the project.
- To exclude a file from Project -> select the file -> Right Click -> select “Exclude file(s) from current configuration” or Remove file from the Project. The former option just exclude from the project and latter option will remove the file from project.
- Replace the contents of "libc_syscalls.c" file in the project with the contents of "libc_syscalls.c" file in the zip. This file has definition of_sbrk() needed for Arm GCC compiler in addition to content what already present in it.
- After completing the above steps, compile the project.
- The project should compile successfully.
Running the Demo:
- Perform Prerequisites, Configure the project to use Arm GCC toolchain, Compile the project using Arm GCC Toolchain and Setting up SAM D21 Xplained Pro Evaluation Kit steps mentioned above, if not done already.
- Open the Tera Term terminal application on the PC (from the Windows Start menu by pressing the Start button).
- Connect to the EDBG Virtual COM port and configure the baud rate to 115200.
- Build and Program the application using the MPLAB X IDE.
Results
- The console displays the message stating whether voltage at PA04 is lower or greater than the internal bandgap voltage (1.1 V)
- LED0 toggles when comparison is
done.
Conclusions
This guide demonstrated building an MPLAB Harmony v3 peripheral Libraries (PLIBs) example with Arm GCC Toolchain. The same approach can be followed for any other Harmony v3 project.