3.4.1.1 ATWINC1510 Firmware Upgrade
Description
The SAM-IoT WA V2 Development Application uses ATWINC1510-MR210PB IEEE 802.11 b/g/n module to enable cloud connectivity. The application's functioning requires the ATWINC1510 module to have firmware compatible with the WiFi software stack running on the SAM-IoT microcontroller. To enable this compatibility, the ATWINC1510 module is updated with the firmware compatible with WiFi software running in the latest released demo.
The root certificates to identify the IoT node to the AWS cloud platform are programmed in the non-volatile memory of the ATWINC1510 module.
If the user is following readme other than TPDS, complete below step before proceeding with Serial Bridge Application to upgrade ATWINC1510 Firmware.
Running the Utility
- Click on winc_provisioner.bat, it
automatically downloads WINC firmware package and runs a command using a command
prompt.
- Select SAM IoT V2 COM PORT from the drop
down and click OK

- Wait till verify passed message comes up
as shown below and then click on enter to close he command prompt, if fails, reconnect the
board and try.