4.1 Configuration Changes
As soon as the analog comparator settings are modified, the output of the analog comparator is masked for the time that its output may be invalid. Depending on the user application the following function calls may require the comparator output to be valid before continuing:
The following code may be used to check if the comparator output is valid before continuing:
*while((acc_get_interrupt_status(ACC) & ACC_ISR_MASK) == ACC_ISR_MASK) {* }