3.1 ECC608-TNGHNT Configuration Zone
The ECC608-TNGHNT configuration is fixed and cannot be modified by the customer. Relevant information about how the device is configured is shown below or in the slot information.
Device Configuration Information
- The serial number for each device is unique and stored in bytes [0:3, 8:12]. Bytes [0:1] are 0x01 0x23 and byte [8] is 0x6F. All other bytes are unique.
- The default 7-bit I2C
address is 0x60. The I2C address
can be overwritten using the
UpdateExtracommand.Important: The default I2C address of the ECC608-TNGHNT is identical to that of the standard ATECC608 Device. - The I/O levels are set to a fixed reference level; therefore, the host processor can operate at a lower voltage than the ECC608-TNGHNT device.
- The Watchdog Timer (WDT) is set to a maximum time-out of 1.3s.
- The use of an I/O protection key is enabled with the key stored in Slot 6.
- For the ECC608-TNGHNT, the following individual slots have been configured to be slot lockable: Slots 0, 3-4, 6 and 8.
- Monotonic counters are available for use by the system and are not attached to any keys.
- The Health Test Failure bit is cleared after any time that a command fails as a result of a health test failure. If the failure symptom is transient, the command may pass when run a second time.