6.1.9 UpdateExtra Command
The UpdateExtra command is used to update the UpdateExtra and
UpdateExtraAdd bytes, bytes 84 and 85 respectively, in the Configuration zone. These
bytes can only be updated by this command. These bytes are one-time updatable bytes and
can only be updated if the current value is 0x00. Trying to update this byte if the
value is not 0x00 will result in an error.
For the ATECC608C-TNGTLS device, the UpdateExtraAdd byte (byte 85) has been configured to be an alternate I2C address.