1.5.3.5 mchp_mat_inverse_q31()
mchp_status mchp_mat_inverse_q31 (const mchp_matrix_instance_q31 * src, mchp_matrix_instance_q31 * dst)
Q31 matrix inverse.
| in | src |
points to the instance of the input Q31 matrix structure. |
| out | dst |
points to the instance of the output Q31 matrix structure. |
The function returns MCHP_MATH_SIZE_MISMATCH, if the dimensions do not match. If the input matrix is singular (does not have an inverse), then the algorithm terminates and returns error status MCHP_MATH_SINGULAR. |