8.7 Resolved Issues
(Ask a Question)The following table lists the customer-reported defects and enhancement requests resolved in Libero SoC v2022.1 that have case numbers. Resolution of previously reported “Known Issues and Limitations” are also noted in this table.
| Case Number | Summary | Resolution |
|---|---|---|
| 00770055 | PLL configuration with External Feedback generates errors during Place and Route. | Configurator-generated constraints are fixed to not
add -pll_feedback and -pll_output when
feedback source is Dedicate Pad. |
| 00758973,00783075 | FCCC auto-derived constraints produce errors during compile. | An issue with path search between the PLL output and PLL feedback has been fixed. |
| 00771288, 00909815 | KIT_LICENSE_IP: Device Family parameter/configurator issue with MPF300T devices with Gold license. | The device mapping information is now passed correctly to COREFIFO when a Gold license is used. |
| 00780224 | When the FDDR/MDDR is configured to support 4GB, it cannot access the entire 32-bit AXI address range. Designs that do not map the MSB of the 32-bit AXI address to the DDR memory address are not affected (that is, if the AXI address does not exceed a 2GB address space). | For more information, see section DDR Memory Controller Change of Memory Density . |
| 00805467 | New line character is not seen as a separator between two SDC commands in the SDC file. | Interpretation of commands between curly braces in SDC files has been fixed. |
| 00815661 | DRC violations message in SSN Analyzer. | For DRC violations, DRC warning messages will be shown to the noise margin and excluded IO page. |
| 00813594 | Enhancement request on Libero support for RHEL 7.9. | Starting with v2022.1, Libero SoC will be supported on RHEL/CentOS 7.9. |
| 00827297 | Library logical name WORK not treated as current working library by Synplify Pro. |
Synplify Pro S-2021.09M adds a new option to treat the VHDL library logical name “work” as the current library.
|
| 00843870 | Synthesis error on inferred RAM. | When Synplify Pro promoted a GND net to global, Libero failed "per DRC, static values are expected to be assigned to this pin." Now Synplify Pro will not promote the GND pin to Global. |
| 00845159,00803696 | Synthesis error occurs when trying to open encrypted HDL files on 11th generation processor machines. | Encrypted designs are supported and will pass successfully with Synplify Pro S2021.09M on 11th generation processor machines. |
| 00847579 | Error message with a specific clock signal during Multipass Place and Route. | Compare failed error message was
reported in the iteration summary report because the
Frequency field was removed from timing
reports. Multipass Place and Route now evaluates the best seed by Worst
Slack. |
| 00849469 | PF_SOC: MSS: QSPI I/Os do not support 1.8V. | Updated DRC for all peripherals. |
| 00850843 |
SmartDebug enhancement request: Export embedded non-volatile memory (eNVM) and secure non-volatile memory (sNVM) to file. | For more information, see section SmartDebug Option to Export Contents of eNVM and sNVM. |
| 00852603 | SmartTime reports unreasonably high clock generation time. | Fixed an issue when calculating the short path for some gated clock designs. |
| 00853926 | Signal integrity settings from I/O Editor have no effect on design implementation. | This issue affected the I/O settings of lanes and
REFCLK of transceivers when replication was enabled
in Place and Route. Rerun Place and Route in Libero SoC v2022.1. |
| 00859317 | PF_PCIE issue with PCIE0 BAR0. | Fixed settings when BAR0 is enabled
for the PCIe0 controller, but disabled for the PCIe1 controller. |
| 00859778, 00853856, 00780930 | Identify Debugger crashes on 11th generation processor machines. | Identify Debugger invokes successfully to communicate with the board. |
| 00865046 | Synthesis error in the customer design. | Synthesis error related to Not enough net
bundle has been fixed. |
| 00877502, 00877508 | PF_PCIE: PolarFire PCIe1 Slot clock and ASPM L1 configuration settings are not updated as per the PCIe GUI configuration | Updated register settings. |
| 00883697 | PCIe model does not drive to Elec-Idle ('z') | IGLOO2, SmartFusion2, and RTG4 simulation has been
enhanced to support tri-state 'z' behavior on PCIe Tx lines. Using the
vsim command, users can choose PCIe block to drive
between a common voltage signal (typically '0' by default) and Tri state
('z'). |
| 00896689 | For RTG4 devices, the Program and
Connectivity Tool crashes due to the missing library
libpng12-0:i386. | This library is present after installing Libero 2022.1. |
| 00888205 | Remove the empty configuration file generated by configurator | Empty configuration file is no longer generated |
| 00897728 | SynplifyPro incorrectly modeling Global. | Clock buffer delays have been updated in Synplify Pro S2021.09M. |
| 00900308 | PF_CCC: PolarFire CCC GUI configuration difference between 2021.2 and 2021.3 | Fixed issue with output frequency computation. |
| 00913713 | KIT_LICENSE_IP: COREFIFO ECC flags not available in Smart Design with Gold license. | The device mapping information is now passed
correctly to COREFIFO when a Gold license is
used. |
| 00925061 | Libero batch mode crashes when Internet access is disabled. | When the Internet preferences are disabled, a message is not issued via a dialog box in batch mode. |
| 00967427 |
For SmartFusion2 and IGLOO2 Libero designs, if the customer selected an eNVM component only in bitstream along with the sanitize all eNVM pages option, the output of Generate Bitstream, Export Bitstream, and Export FlashPro Express Job produces incorrect bitstream file where running ERASE action will program eNVM instead of sanitizing eNVM. | This issue is fixed in Libero v2022.2. |
| 493642-2812294750 | Synplify support for nested interfaces. | Removed reference to VHDL nested interface from the Synplify Pro User Guide. It is not supported by Synplify Pro. |
| 493642-2816309250 | SmartPower does not support VDDAUX
set to 3.3v in PolarFire. | Added 2.5v and 3.3v selection for VDDAUX rail in Verify power right click options. |
| 493642-2826151737 | Exporting SmartTime User SETs. | For more information, see section SmartTime – User SET. |
| 493642-2833553813 | SmartDesign BIF port name change issue. | For more information, see section SmartDesign Enhancements. |
| 493642-2847447625 | PF_PCIE: Incorrect use model for
PERSTn when RootPort. | For more information, see section PCIe Root-port Capability to Work with APB Initiator to Control the PERSTn Output to Downstream PCIe Endpoints. |
| 493642-2892634270 | IGLOO2 CCC external feedback, Place and Route error messages. | Regenerating constraints from the CCC Configurator
will not add -pll_feedback and
-pll_output when feedback source is
Dedicate Pad. Place and Route will not
encounter No path found messages. |
The following table lists the customer-reported defects and enhancement requests resolved in Libero SoC v2022.1 that do not have case numbers. Resolution of previously reported “Known Issues and Limitations” are also noted in this table.
| Summary | Resolution |
|---|---|
| Problem to close Timing on MPF500 Design, very long PnR Times. | The issue is no longer observed in the current release. |
| PF_SYSTEM_SERVICES: Simulations fail for system services when they look for sNVM.mem in Linux. | PF_SYSTEM_SERVICES simulation model was updated to work in the Linux environment when sNVM contents are passed. |
| In the PolarFire DDR4 Configurator, you can enable both ECC and DM at the same time. These should be mutually exclusive selections. | Added a DRC so that the ECC and DM are mutually exclusive. |
| FlashPro Express fails to perform any programming action using FlashPro 6 using the SPI Target interface. The JTAG interface is not affected. | Fixed an issue during programmer update where the programmer was not closed properly causing subsequent operations to fail. |
| RTG4: Assertion Failed in /po_nwkiutil.cxx, line 7732 during Place and Route. | An instance of the RGRESET macro routes a triplicated fabric signal to a row global buffer to create a local reset. The three input bits must be driven by three separate logic cones replicating the paths from the source registers. |
| Output Delay constraint causes IOFF4 error. | The automatic I/O register combining will check whether a timing constrained path already contains a I/O register inserted by Compile, and avoid combining such I/O or registers in the process. |
| Support PolarFire MPF300 ES Kit based devices with Silver license. | For more information, see section MPF300TS_ES Device Licenses. |
| PF_XCVR: PF_TXPLL: Update TXPLL Spread Spectrum Clock Generation (SSCG) user interface. | Renamed labels in the Spread Spectrum tab of the
TXPLL and CCC configurators as follows:
|
| Synthesis warning message from RTG4 FCCC. | Warning message is no longer observed in the synthesis report. |
Crash: Signal 011 error in
m_generic.exe.
ID:map202103act/060/m_generic.exe | The SynplifyPro crash related to DSP mapping is been fixed. |
| Erase FABRIC digest when erasing Fabric in ERASE action. | Updated ERASE action to also erase Fabric digest when erasing Fabric. |
| USB I/Os not supported 1.8V/2.5V. | Added 2.5V and 1.8V as supported voltages for USB in the MSS configurator. |
| MMUART I/Os not supported 1.2V/1.5V/18V/3.3V. | Updated DRC for I/O voltage supported for peripherals. |
| PF_CCC: Clock Uncertainty: Inclusion of jitter in CCC/PLL auto-constraint generation. | For more information, see section New Timing Constraint Flow to Automatically Account for Global Clock Jitter. |