2.6 Migrating Designs to Libero SoC
(Ask a Question)2.6.1 Core Enhancements and Upgrades
(Ask a Question)The following table lists core enhancements and upgrades in Libero SoC v2024.2. For more information about updating a core version, see section Updating a Core Version.
| Core | 2024.2 Version | Status | Comments |
|---|---|---|---|
| PF_DDR3 | 2.4.124 | Production |
See section “CK/CA additive offset” Parameter in the Training IP of DDR Controllers. |
| PF_DDR4 | 2.5.113 | Production |
See section “CK/CA additive offset” Parameter in the Training IP of DDR Controllers. |
| PF_IOD_TX_CCC | 1.0.130 | Production | See section Phase Direction Parameter for BCLK/SCLK Alignment. |
| PF_IOD_GENERIC_RX | 2.1.113 | Production | See section Phase Direction Parameter for BCLK/SCLK Alignment. |
| PF_LPDDR3 | 2.3.120 | Production |
See section “CK/CA additive offset” Parameter in the Training IP of DDR Controllers. |
| PF_RGMII_TO_GMII | 1.3.110 | Production | PF_RGMII_TO_GMII has been repackaged with the new version of the PF_IOD_GENERIC_RX core. |
| SmartFusion2/IGLOO2 TAMPER | 2.1.301 | Production | See section SmartFusion2 and IGLOO2. |
| SmartFusion2/IGLOO2 TAMPER2 | 2.1.301 | Production | See section SmartFusion2 and IGLOO2. |
| SmartFusion2/IGLOO2 TAMPER3 | 2.1.301 | Production | See section SmartFusion2 and IGLOO2. |
2.6.2 Updating a Core Version
(Ask a Question)- Download the latest version of the core into your vault.
-
Upgrade each configured core in your design to the latest version by
right-clicking the core component in the design hierarchy and selecting
Update Component Version. The component is
regenerated automatically.
Important: The Update Component Version option is now available on instances of core components in a SmartDesign canvas as well. In addition, the selected core version is downloaded automatically from the Update Component Version dialog itself if needed.
- Review the SmartDesign components and user RTL files in which the core component has been instantiated. If the port-list of the core component is modified after updating to the new core version, right-click the core component's instance in the SmartDesign and select Update Instance to update its port-list. Check for any pin/port disconnections in the SmartDesign or for any new pins exposed on the core component's instance, and then connect them or tie them off as needed and regenerate the SmartDesign component.
- Build Design Hierarchy and Derive the Timing Constraints again from the Constraint Manager tool to use the latest generated core timing constraints.
- Rerun the design flow.