2.1.3 AES Command
The AES command supports a 128-bit Advanced Encryption
Standard - Electronic Code Book (AES- ECB) encryption, AES-ECB decryption and calculates
the GFM of the input data. An operation for encryption and decryption is performed for
16 bytes at a time.
This command supports the selection of a 16-byte AES key, which can be taken from any of the below sources:
- TempKey – A feature used to select one of the 16 bytes as a key from TempKey
- Data Slot – A feature used to select one of the 16 bytes as a key from a data slot
The value returned from the device is the encrypted/decrypted data, GFM data or an error code.