2.1.2 WPAN_Task Function
C
bool WPAN_Task(void)Summary
Runs the WPAN Task scheduler
Description
This function invokes the corresponding task functions of the MCL, PHY, and PAL Using the MAC software package it is required to call this function frequently supporting a round robin approach ensures that the different layers state machines are served, and their queues are processed. This routine must be called from the RTOS Task function in case of any RTOS is used.
Precondition
WPAN_Init() should have been called before calling this function.
Parameters
None.
Returns
Boolean true if an event was processed otherwise false.
Example
WPAN_Task();
Remarks
This routine must be called before any of the MAC-WPAN function is called