2.1.1 WPAN_Init Function
C
MAC_Retval_t WPAN_Init(void)Summary
Initialization of MAC Layer
Description
This function initializes the MAC Layer. This is function is called to Initializes all stack resources including the microcontroller and transceiver using functions provided by the PHY and the PAL.
Precondition
PHY_Init() should have been called before calling this function.
Parameters
None.
Returns
MAC_SUCCESS - if MAC initialized successfully
FAILURE - otherwise
Example
MAC_Retval_t retVal = FAILURE;
retVal = WPAN_Init();
if (MAC_SUCCESS != retVal)
{
while(1);
}Remarks
This routine must be called before any of the MAC-WPAN function is called