18.3.5 Makefile Interface
To remove all target files for a given configuration:
- Change directory to $PROJECT_DIR.
make -f nbproject/Makefile-debugOption.mk SUBPROJECTS= .clean-conf
This will clean the target files for the debugOption configuration.
To remove all target files for all configurations:
- Change directory to $PROJECT_DIR.
make clobber
To run the Makefile for a given configuration:
- Change directory to $PROJECT_DIR.
- Set environment variables to override values in the Make process.
make -f nbproject/Makefile-$CONFIGURATION_NAME.mk SUBPROJECTS= .build-confwhere $CONFIGURATION_NAME is the name of the configuration Makefile to be run.
For a configuration called default:
make -f nbproject/Makefile-default.mk SUBPROJECTS= .build-conf
The output for a configuration is one of the debug .elf files. The
production image will be a .hex file.
$PROJECT_NAME is the name of the project.
dist/$CONFIGURATION_NAME/debug/$PROJECT_NAME.debug.elf
dist/$CONFIGURATION_NAME/production/$PROJECT_NAME.production.hex