3.3.3 Enable the Module Licensing Feature
This section describes how to enable specific HSM module features.
Feature Enabling Tool (fet) utility, the module must be switched to
the pre-initialization mode.To run the custom firmware created for the SPPS system (SEE Machine), the module must have the
"SEE Activation (EU+10)" feature enabled, as shown in sample Figure 3-4. Feature status of the module can be
checked or activated using fet.
Choose option one and activate the features listed on your Activator Card (see section Activator Card and Feature Licensing (nCipher)). The fet auto-detects the card and performs activation. New activation status is printed on the screen.
If your Activator Card does not include the "SEE Activation (EU+10)" feature, it might have been provided to you in a separate file. The file name includes the module serial number, for example: USProdCGT3-01253481317_SEEUE_8FD6-2609-F7A2.txt
This file can be used during activation independently from the Activator Card by selecting option two.
If you plan to use advanced security features in Microchip devices, such as ECC PUF key modes, make sure that the "Elliptic Curve algorithms" and "Elliptic Curve MQV" are activated as shown in the preceding example.
fet. Licensing feature
reset can only be done at the factory.