| 0x00 | PIN0 | Event actions will be
executed on pin 0 |
| 0x01 | PIN1 | Event actions will be
executed on pin 1 |
| 0x02 | PIN2 | Event actions will be
executed on pin 2 |
| 0x03 | PIN3 | Event actions will be
executed on pin 3 |
| 0x04 | PIN4 | Event actions will be
executed on pin 4 |
| 0x05 | PIN5 | Event actions will be
executed on pin 5 |
| 0x06 | PIN6 | Event actions will be
executed on pin 6 |
| 0x07 | PIN7 | Event actions will be
executed on pin 7 |
| 0x08 | PIN8 | Event actions will be
executed on pin 8 |
| 0x09 | PIN9 | Event actions will be
executed on pin 9 |
| 0x0A | PIN10 | Event actions will be
executed on pin 10 |
| 0x0B | PIN11 | Event actions will be
executed on pin 11 |
| 0x0C | PIN12 | Event actions will be
executed on pin 12 |
| 0x0D | PIN13 | Event actions will be
executed on pin 13 |
| 0x0E | PIN14 | Event actions will be
executed on pin 14 |
| 0x0F | PIN15 | Event actions will be
executed on pin 15 |
| 0x10 | PIN16 | Event actions will be
executed on pin 16 |
| 0x11 | PIN17 | Event actions will be
executed on pin 17 |
| 0x12 | PIN18 | Event actions will be
executed on pin 18 |
| 0x13 | PIN19 | Event actions will be
executed on pin 19 |
| 0x14 | PIN20 | Event actions will be
executed on pin 20 |
| 0x15 | PIN21 | Event actions will be
executed on pin 21 |
| 0x16 | PIN22 | Event actions will be
executed on pin 22 |
| 0x17 | PIN23 | Event actions will be
executed on pin 23 |
| 0x18 | PIN24 | Event actions will be
executed on pin 24 |
| 0x19 | PIN25 | Event actions will be
executed on pin 25 |
| 0x1A | PIN26 | Event actions will be
executed on pin 26 |
| 0x1B | PIN27 | Event actions will be
executed on pin 27 |
| 0x1C | PIN28 | Event actions will be
executed on pin 28 |
| 0x1D | PIN29 | Event actions will be
executed on pin 29 |
| 0x1E | PIN30 | Event actions will be
executed on pin 30 |
| 0x1F | PIN31 | Event actions will be
executed on pin 31 |