6.1 Device Addressing
Accessing the device requires an 8-bit device address byte following a Start condition to enable the device for a read or write operation. Since multiple client devices can reside on the serial bus, each client device must have its own unique address so the host can access each device independently.
The Most Significant four bits of the device address byte is referred to as
the device type identifier. The device type identifier ‘1010’ (Ah) is
required in bits 7 through 4 of the device address byte (see Table 6‑1).
Following the 4-bit device type identifier are the hardware client address bits, A2 and A1.
These bits can be used to expand the address space by allowing up to four Serial EEPROM
devices on the same bus. The A2 and A1 values must correlate with the voltage level on the
corresponding hardwired device address input pins A2 and A1. The A2 and A1 pins use an
internal proprietary circuit that automatically biases it to a logic ‘0’
state if the pin is allowed to float. In order to operate in a wide variety of application
environments, the pull‑down mechanism is intentionally designed to be somewhat strong. Once
these pins are biased above the CMOS input buffer’s trip point (~0.5 x VCC), the
pull-down mechanism disengages. Microchip recommends connecting the A2 and A1 pin to a
known state whenever possible.
Following the A2 and A1 hardware client address bits is bit A16 (bit 1 of the device address byte), which is the Most Significant bit of the memory array word address. Refer to Table 6-1 to review the bit position.
The eighth bit (bit 0) of the device address byte is the Read/Write Select bit. A read operation is initiated if this bit is high and a write operation is initiated if this bit is low.
Upon the successful comparison of the device address byte, the AT24CM01 will return an ACK. If a valid comparison is not made, the device will NACK.
| Package | Device Type Identifier | Hardware Client Address Bits | Most Significant Bit of the Word Address | R/W Select | ||||
|---|---|---|---|---|---|---|---|---|
| Bit 7 | Bit 6 | Bit 5 | Bit 4 | Bit 3 | Bit 2 | Bit 1 | Bit 0 | |
| SOIC, SOIJ, TSSOP, WLCSP | 1 | 0 | 1 | 0 | A2 | A1 | A16 | R/W |
For all operations except the current address read, two 8‑bit word address bytes must be transmitted to the device immediately following the device address byte. The word address bytes consist of the remaining 16 bits of the 17-bit memory array word address and are used to specify which byte location in the EEPROM to start reading or writing.
The first word address byte contains the next eight bits of the word address (A15 through A8) in bit positions seven through zero, as seen in Table 6-2. Upon completion of the first word address byte, the AT24CM01 will return an ACK.
| Bit 7 | Bit 6 | Bit 5 | Bit 4 | Bit 3 | Bit 2 | Bit 1 | Bit 0 |
|---|---|---|---|---|---|---|---|
| A15 | A14 | A13 | A12 | A11 | A10 | A9 | A8 |
Next, the second word address byte is sent to the device, which provides the remaining eight bits of the word address (A7 through A0). Upon completion of the second word address byte, the AT24CM01 will return an ACK. See Table 6-3 to review these bit positions.
| Bit 7 | Bit 6 | Bit 5 | Bit 4 | Bit 3 | Bit 2 | Bit 1 | Bit 0 |
|---|---|---|---|---|---|---|---|
| A7 | A6 | A5 | A4 | A3 | A2 | A1 | A0 |