1.3 EEPROM Emulator Library Read/Write
This application example demonstrates how to read and write to the Emulated EEPROM memory space using the EEPROM Emulator library.
Description
This example uses EEPROM Emulator library to read and write to the NVM Emulated EEPROM memory space. The application first checks if the library was initialized successfully or not. When running the application for the first time, the EEPROM Emulator memory space will be formatted by the application. The application then writes data to EEPROM memory space using the APIs provided by the EEPROM Emulator library and then reads the data back and compares it with the written data.
Downloading and Building the Application
To clone or download this application from GitHub, go to the main page of this repository and then click Clone button to clone this repository or download as zip file.
Path of the application within the repository is apps/library/eeprom_emulator/eeprom_emulator_read_write.
To build the application, refer to the following table and open the project using its IDE.
| Project Name | Description |
|---|---|
| pic32mx470_curiosity.X | MPLAB X project for Curiosity PIC32MX470 Development Board |
Setting Up the Hardware
The following table shows the target hardware for the application projects.
| Project Name | Description |
|---|---|
| pic32mx470_curiosity.X | Curiosity PIC32MX470 Development Board |
Setting Up Curiosity PIC32MX470 Development Board
- No additional hardware is required to run this demo
- Connect the Debug USB port on the board to the computer using a micro USB cable
Running the Application
- Build and program the application using its IDE.
- LED indicates success or failure:
- The LED is turned ON when the value read from the Emulated EEPROM memory region matches with the written value
| Board | LED Name |
|---|---|
| Curiosity PIC32MX470 Development Board | LED1 |