1.11 I2C EEPROM AT24 Driver - EEPROM Read/Write
This example application shows how to use the AT24 driver to perform read and write operations on AT24 series of EEPROM.
Description
This example uses the AT24 driver to communicate with I2C based external AT24 series EEPROMs to perform write and read operations in Bare-Metal environment.
Downloading and Building the Application
To clone or download this application from GitHub, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/driver/i2c_eeprom/at24/at24_eeprom_read_write/firmware.
To build the application, refer to the following table and open the project using its IDE.
| Project Name | Description |
|---|---|
| pic32mx470_curiosity.X | MPLAB X project for Curiosity PIC32MX470 Development Board |
| pic32mx_xlp_sk.X | MPLAB X project for PIC32MX274 XLP Starter Kit |
Setting Up the Hardware
The following table shows the target hardware for the application projects.
| Project Name | Description |
|---|---|
| pic32mx470_curiosity.X | Curiosity PIC32MX470 Development Board |
| pic32mx_xlp_sk.X | PIC32MX274 XLP Starter Kit |
Setting Up Curiosity PIC32MX470 Development Board
- To run the demo, the following additional hardware is required:
- Connect mini USB cable to the Debug USB connector (J3) on the board to the computer
- Install the EEPROM 3 Click board onto the mikroBUS socket J5
of Curiosity PIC32MX470 Development
BoardNote: Ensure that the series resistors on the mikroBUS headers are of value 0Ω.
Setting Up PIC32MX274 XLP Starter Kit
- To run the demo, the following additional hardware is required:
- Connect micro USB cable to the Debug USB connector (J9) on the board to the computer
- Install the EEPROM 3 Click board onto the mikroBUS socket J5 of PIC32MX274 XLP Starter Kit
Running the Application
- Build and program the application using its IDE.
- The LED is turned ON when the data read from EEPROM matches with the written data.
| Board | LED Name |
|---|---|
| Curiosity PIC32MX470 Development Board | LED1 |
| PIC32MX274 XLP Starter Kit | LED1 (RED) |