1.13 SPI Driver Asynchronous - Self-Loopback Multi Client

This example demonstrates how to use the SPI driver in Asynchronous mode to achieve self-loopback between multiple clients.

Description

  • This example writes and reads back the same data (self-loopback) for two different clients connected over the same SPI bus by using the multi-client feature of the driver
  • It uses the request (write and read request) queuing feature of the asynchronous driver and does not waste CPU bandwidth in waiting for previous request completion
  • The example also demonstrates how to setup two different client transfers at different baud rates
  • This example performs self-loopback only once after a power-on reset
  • Success is indicated when a successful self-loopback is reported by both the clients
  • After the loopback test is complete, the application remains in the Idle state

Downloading and Building the Application

To clone or download this application from GitHub, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.

Path of the application within the repository is apps/driver/spi/async/spi_self_loopback_multi_client/firmware.

To build the application, refer to the following table and open the project using its IDE.

Project NameDescription
pic32mx_xlp_sk.XMPLAB X project for PIC32MX274 XLP Starter Kit

Setting Up the Hardware

The following table shows the target hardware for the application projects.

Project NameDescription
pic32mx_xlp_sk.XPIC32MX274 XLP Starter Kit

Setting Up PIC32MX274 XLP Starter Kit

  • Connect micro USB cable to the Debug USB connector (J9) on the board to the computer
  • Use jumper wire to connect Pin 5 of J5 to Pin 6 of J5
    • SDI1 is mapped to RC8, which is routed to Pin 5 of J5
    • SDO1 is mapped to RA8, which is routed to Pin 6 of J5

Running the Application

  1. Build and program the application using its IDE.
  2. The LED is turned ON on Success.
Refer to the following table for LED name:
BoardLED Name
PIC32MX274 XLP Starter KitLED1 (RED)