1 Harmony 3 Driver and System Service Application Examples for PIC32MX Family

The following applications are provided to demonstrate the typical or interesting usage models of one or more drivers and system services.

NameDescription
Console Debug System Service Using UARTThis example application demonstrates the UART based console and debug system service
Console Debug System Service Using USBThis example application demonstrates the USB based console and debug system service
EEPROM Emulator Library Read/WriteThis application example demonstrates how to read and write to the Emulated EEPROM memory space using the EEPROM Emulator library
FAT File System Using NVM MediaThis application shows an example of implementing a FAT disk in the device internal Flash memory
FAT File System Using SDSPI MediaThis application shows an example of using the MPLAB Harmony File System to access and modify the contents of a SD card using the SDSPI driver and the SPI PLIB
FAT File System Using SPI Driver With SDSPI MediaThis application shows an example of using the MPLAB Harmony File System to access and modify the contents of a SD card using the SDSPI and a SPI driver
FreeRTOS BasicThis example application demonstrates context switching between different tasks having different priorities
FreeRTOS Task NotificationThis example application is to illustrate the FreeRTOS Task Notification feature which is used as a lightweight binary semaphore
I2C Driver Asynchronous - I2C EEPROMThis example application shows how to use the I2C driver in Asynchronous mode to perform operations on the EEPROM
I2C Driver Synchronous - I2C EEPROMThis example application shows how to use the I2C driver in Synchronous mode to perform operations on the EEPROM
I2C EEPROM AT24 Driver - EEPROM Read/WriteThis example application shows how to use the AT24 driver to perform read and write operations on AT24 series of EEPROM
SPI Driver Asynchronous - Multi InstanceThis example demonstrates how to use multiple instances of the SPI driver in Asynchronous mode to communicate with multiple EEPROMs
SPI Driver Asynchronous - Self-Loopback Multi ClientThis example demonstrates how to use the SPI driver in Asynchronous mode to achieve self-loopback between multiple clients
SPI Driver Synchronous - Multi InstanceThis example demonstrates how to use multiple instances of the SPI driver in Synchronous mode to communicate with multiple EEPROMs in an RTOS environment
SPI EEPROM AT25 Driver - EEPROM Read/WriteThis example application shows how to use the AT25 driver to perform read and write operations on AT25 series of EEPROM
Time System Service Multi ClientThis example application demonstrates the multi-client system timer functionality
USART Driver Asynchronous - USART EchoThis example echoes the received characters over the console using the USART driver in Asynchronous mode
USART Driver Synchronous - USART EchoThis example echoes the received characters over the console using the USART driver in Synchronous mode