| AP_VER=Algorithm Plugin Version. |
| AREAS_TO_PROGRAM=The following memory
area(s) will be programmed: |
| AREAS_TO_READ=The following memory area(s)
will be read: |
| AREAS_TO_VERIFY=The following memory
area(s) will be verified: |
| BLANK_CHECK_COMPLETE=Blank check complete,
device is blank. |
| BLANK_CHECKING=Blank Checking... |
| BOOT_CONFIG_MEMORY=boot config
memory. |
| BOOT_VER=Boot Version. |
| BOOTFLASH=boot flash. |
| BP_CANT_B_DELETED_WHEN_RUNNING=software
breakpoints cannot be removed while the target is running. The selected
breakpoint will be removed the next time the target halts. |
| CANT_CREATE_CONTROLLER=Unable to find the
tool controller class. |
| CANT_FIND_FILE=Unable to locate file
%s. |
| CANT_OP_BELOW_LVPTHRESH=The voltage level
selected %f, is below the minimum erase voltage of %f. The operation
cannot continue at this voltage level. |
| CANT_PRESERVE_PGM_MEM=Unable to preserve
program memory: Invalid range Start = %08x, End = %08x. |
| CANT_READ_REGISTERS=Unable to read target
register(s). |
| CANT_READ_SERIALNUM=Unable to read the
device serial number. |
| CANT_REMOVE_SWPS_BUSY=The ICE 4 is
currently busy and cannot remove software breakpoints at this time.
|
| CHECK_4_HIGH_VOLTAGE_VPP=CAUTION: Check
that the device selected in MPLAB IDE (%s) is the same one that is
physically attached to the debug tool. Selecting a 5V device when a 3.3V
device is connected can result in damage to the device when the debugger
checks the device ID. Do you wish to continue? |
| CHECK_PGM_SPEED=You have set the program
speed to %s. The circuit on your board may require you to slow the speed
down. Please change the setting in the tool properties to low and try
the operation again. |
| COMM_PROTOCOL_ERROR=A communication error
with the debug tool has occurred. The tool will be reset and should
re-enumerate shortly. |
| COMMAND_TIME_OUT=ICE 4 has timeout out
waiting for a response to command %02x. |
| CONFIGURATION=configuration. |
| CONFIGURATION_MEMORY=configuration
memory. |
| CONNECTION_FAILED=Connection
Failed. |
| CORRUPTED_STREAMING_DATA=Invalid streaming
data has been detected. Run time watch or trace data may no longer be
valid. It is recommended that you restart your debug session. |
| CPM_TO_TARGET_FAILED=An exception occurred
during ControlPointMediator.ToTarget(). |
| DATA_FLASH_MEMORY=Data Flash
memory. |
| DATA_FLASH=data flash. |
| DEBUG_INFO_PGM_FAILED=Could not enter debug
mode because programming the debug information failed. Invalid
combinations of config bits may cause this problem. |
| DEBUG_READ_INFO=Reading the device while in
debug mode may take a long time due to the target oscillator speed.
Reducing the range that you'd like to read (under the ICE 4 project
properties) can mitigate the situation. The abort operation can be used
to terminate the read operation if necessary. |
| DEVICE_ID_REVISION=Device Id
Revision. |
| DEVICE_ID=Device Id. |
| DEVID_MISMATCH=Target Device ID (0x%x) is
an Invalid Device ID. Please check your connections to the Target
Device. |
| DISCONNECT_WHILE_BUSY=The tool was
disconnected while it was busy. |
| EEDATA_MEMORY=EEData memory. |
| EEDATA=EEData. |
| EMULATION_MEMORY_READ_WRITE_ERROR=An error
occurred while trying to read/write MPLAB's emulation memory:
Address=%08x. |
| END=end. |
| ENSURE_SELF_TEST_READY=Please ensure the
RJ-11 cable is connected to the test board before continuing. |
| ENSURE_SELF_TEST_READY=Please ensure the
RJ-11 cable is connected to the test board before continuing. Would you
like to continue? |
| ENV_ID_GROUP=Device Identification. |
| ERASE_COMPLETE=Erase successful. |
| ERASING=Erasing... |
| FAILED_2_PGM_DEVICE=Failed to program
device. |
| FAILED_CREATING_COM=Unable create
communications object (RI4Com). |
| FAILED_CREATING_DEBUGGER_MODULES=Initialization failed: Failed creating
the debugger module. |
| FAILED_ESTABLISHING_COMMUNICATION=Unable to
establish tool communications. |
| FAILED_GETTING_DBG_EXEC=A problem occurred
while trying to load the debug executive. |
| FAILED_GETTING_DEVICE_INFO=Initialization
failed: Failed while retrieving device database (.pic)
information. |
| FAILED_GETTING_EMU_INFO=Initialization
failed: Failed getting emulation database information. |
| FAILED_GETTING_HEADER_INFO=Initialization
failed: Failed getting header database information. |
| FAILED_GETTING_PGM_EXEC=A problem occurred
while trying to load the program executive. |
| FAILED_GETTING_TEX=Unable to obtain the
ToolExecMediator. |
| FAILED_GETTING_TOOL_INFO=Initialization
failed: Failed while retrieving tool database (.ri4)
information. |
| FAILED_INITING_DATABASE=Initialization
failed: Unable to initialize the too database object. |
| FAILED_INITING_DEBUGHANDLER=Initialization
failed: Unable to initialize the DebugHandler object. |
| FAILED_PARSING_FILE=Failed to parse
firmware file: %s. |
| FAILED_READING_EMULATION_REGS=Failed to
read emulation memory. |
| FAILED_READING_MPLAB_MEMORY=Unable to read
%s memory from %0x08 to %0x08. |
| FAILED_SETTING_SHADOWS=Failed to properly
set shadow registers. |
| FAILED_SETTING_XMIT_EVENTS=Unable to
synchronize run time data semiphores. |
| FAILED_STEPPING=Failed while stepping the
target. |
| FAILED_TO_GET_DEVID=Failed to get Device
ID. Please make sure the target device is attached and try the operation
again. |
| FAILED_TO_INIT_TOOL=Failed to initialize
ICE 4. |
| FAILED_UPDATING_BP=Failed to update
breakpoint:\nFile: %s\naddress: %08x. |
| FAILED_UPDATING_FIRMWARE=Failed to properly
update the firmware. |
| FILE_REGISTER=file register. |
| FIRMWARE_DOWNLOAD_TIMEOUT=ICE 4 timeout out
during the firmware download process. |
| FLASH_DATA_MEMORY=Flash data
memory. |
| FLASH_DATA=flash data. |
| FPGA_VER=FPGA Version. |
| FRCINDEBUG_NEEDS_CLOCKSWITCHING=To use FRC
in debug mode the clock switching configuration bits setting must be
enabled. Please enable clock switching and retry the requested
operation. |
| FW_DOESNT_SUPPORT_DYNBP=The current ICE 4
firmware does not support setting run time breakpoints for the selected
device. Please download firmware version %02x.%02x.%02x or
higher. |
| GOOD_ID_MISMATCH=Target Device ID (0x%x) is
a valid Device ID but does not match the expected Device ID (0x%x) as
selected. |
| HALTING=Halting... |
| HIGH=High. |
| HOLDMCLR_FAILED=Hold in reset
failed. |
| IDS_SELF_TEST_PASSED=ICE4 is functioning
properly. If you are still having problems with your target circuit
please check the Target Board Considerations section of the online
help. |
| IDS_ST_CLKREAD_ERR=Test interface PGC clock
line read failure. |
| IDS_ST_CLKREAD_NO_TEST=Test interface PGC
clock line read not tested. |
| IDS_ST_CLKREAD_SUCCESS=Test interface PGC
clock line read succeeded. |
| IDS_ST_CLKWRITE_ERR=Test interface PGC
clock line write failure. Please ensure that the tester is properly
connected. |
| IDS_ST_CLKWRITE_NO_TEST=Test interface PGC
clock line write not tested. |
| IDS_ST_CLKWRITE_SUCCESS=Test interface PGC
clock line write succeeded. |
| IDS_ST_DATREAD_ERR=Test interface PGD data
line read failure. |
| IDS_ST_DATREAD_NO_TEST=Test interface PGD
data line read not tested. |
| IDS_ST_DATREAD_SUCCESS=Test interface PGD
data line read succeeded. |
| IDS_ST_DATWRITE_ERR=Test interface PGD data
line write failure. |
| IDS_ST_DATWRITE_NO_TEST=Test interface PGD
data line write not tested. |
| IDS_ST_DATWRITE_SUCCESS=Test interface PGD
data line write succeeded. |
| IDS_ST_LVP_ERR=Test interface LVP control
line failure. |
| IDS_ST_LVP_NO_TEST=Test interface LVP
control line not tested. |
| IDS_ST_LVP_SUCCESS=Test interface LVP
control line test succeeded. |
| IDS_ST_MCLR_ERR=Test interface MCLR level
failure. |
| IDS_ST_MCLR_NO_TEST=Test interface MCLR
level not tested. |
| IDS_ST_MCLR_SUCCESS=Test interface MCLR
level test succeeded. |
| IDS_TEST_NOT_COMPLETED=Interface test could
not be completed. Please contact your local FAE/CAE to SAR the
unit. |
| INCOMPATIBLE_FW=The ICE4 firmware in not
compatible with the current version of MPLAB X software. |
| INVALID_ADDRESS=The operation cannot
proceed because the %s address is outside the devices address range of
0x%08x - 0x%08x. |
| MEM_RANGE_ERROR_BAD_END_ADDR=Invalid
program range end address %s received. Please check the manual program
ranges on the debug tool's, "Memories to Program" property page. |
| MEM_RANGE_ERROR_BAD_START_ADDR=Invalid
program range start address %s received. Please check the manual program
ranges on the debug tool's, "Memories to Program" property page. |
| MEM_RANGE_ERROR_END_LESSTHAN_START=Invalid
program range received: end address %s < start address %s. Please
check the manual program ranges on the debug tool's, "Memories to
Program" property page. |
| MEM_RANGE_ERROR_ENDADDR_NOT_ALIGNED=Invalid
program range received: end address %s is not aligned on a proper 0x%x
address boundary. Please check the manual program ranges on the debug
tool's, "Memories to Program" property page. |
| MEM_RANGE_ERROR_STARTADDR_NOT_ALIGNED=Invalid program range received:
start address %s is not aligned on a proper 0x%x address boundary.
Please check the manual program ranges on the debug tool's, "Memories to
Program" property page. |
| MEM_RANGE_ERROR_UNKNOWN=An unknown error
has occurred while trying to validate the user entered memory
ranges. |
| MEM_RANGE_ERROR_WRONG_DATABASE=Unable to
access data object while validating user entered memory ranges. |
| MEM_RANGE_OUT_OF_BOUNDS=The selected
program range, %s, does not fall within the proper range for the memory
area selected. Please check the manual program ranges on the debug
tool's, "Memories to Program" property page. |
| MEM_RANGE_STRING_MALFORMED=The memory
range(s) entered on the, "Memories to Program" property page (%s) is not
formatted properly. |
| MISSING_BOOT_CONFIG_PARAMETER=Unable to
find boot config start/end address in database. |
| MUST_SET_LVPBIT_WITH_LVP=The low voltage
programming feature requires the LVP configuration bit to be enabled on
the target device. Please enable this configuration bit and try the
operation again. |
| NEW_FIRMWARE=Now Downloading new Firmware
for target device: %s |
| NMMR=NMMR |
| NO_DYNAMIC_BP_SUPPORT_AT_ALL=The current
device does not support the ability to set breakpoints while the devices
is running. The breakpoint will be applied prior to the next time you
run the device. |
| NO_PGM_HANDLER=Cannot program software
breakpoints. The program handler has not been initialized. |
| NORMAL=Normal. |
| OP_FAILED_FROM_CP=The requested operation
failed because the device is code protected. |
| OpenIDE-Module-Name=ICE 4 |
| OPERATION_NOT_SUPPORTED=This operation is
not supported for the selected device. |
| OUTPUTWIN_TITLE=ICE 4. |
| PERIPHERAL=Peripheral. |
| POWER_ERROR_NO_9V=The configuration is set
for the tool to provide power to the target but the 9V power jack is not
detected. Please ensure the external 9V barrel jack is connected to the
tool. |
| POWER_ERROR_NO_POWER_SRC=The configuration
is set for the target board to supply its own power but no voltage has
been detected on VDD. Please ensure you have your target powered up and
try again. |
| POWER_ERROR_POWER_SRC_CONFLICT=The
configuration is set for the tool to provide power to the target but
there is voltage already detected on VDD. This is a conflict. Please
ensure your target is not supplying voltage to the tool and try
again. |
| POWER_ERROR_SLOW_DISCHARGE= There seems to
be excessive capacitance on VDD causing a slower system discharge and
shutdown. Consider minimizing overall capacitance loading or use power
from your target to avoid discharge delays. |
| POWER_ERROR_UNKNOWN=An unknown power error
has occurred. |
| POWER_ERROR_VDD_TOO_HIGH=The VDD voltage
desired is out of range. It exceeds the maximum voltage of 5.5V. |
| POWER_ERROR_VDD_TOO_LOW=The VDD voltage
desired is out of range. It is below the minimum voltage of
1.5V. |
| POWER_ERROR_VPP_TOO_HIGH=The VPP voltage
desired is out of range. It exceeds the maximum voltage of
14.2V. |
| POWER_ERROR_VPP_TOO_LOW=The VPP voltage
desired is out of range. It is below the minimum voltage of
1.5V. |
| PRESERVE_MEM_RANGE_ERROR_BAD_END_ADDR=Invalid preserve range end
address %s received. Please check the manual program ranges on the debug
tool's, "Memories to Program" property page. |
| PRESERVE_MEM_RANGE_ERROR_BAD_START_ADDR=Invalid preserve range start
address %s received. Please check the manual program ranges on the debug
tool's, "Memories to Program" property page. |
| PRESERVE_MEM_RANGE_ERROR_END_LESSTHAN_START=Invalid preserve range
received: end address %s < start address %s. Please check the manual
program ranges on the debug tool's, "Memories to Program" property
page. |
| PRESERVE_MEM_RANGE_ERROR_ENDADDR_NOT_ALIGNED=Invalid preserve range
received: end address %s is not aligned on a proper 0x%x address
boundary. Please check the manual program ranges on the debug tool's,
"Memories to Program" property page. |
| PRESERVE_MEM_RANGE_ERROR_STARTADDR_NOT_ALIGNED=Invalid preserve range
received: start address %s is not aligned on a proper 0x%x address
boundary. Please check the manual program ranges on the debug tool's,
"Memories to Program" property page. |
| PRESERVE_MEM_RANGE_ERROR_UNKNOWN=An unknown
error has occurred while trying to validate the user entered preserve
ranges. |
| PRESERVE_MEM_RANGE_ERROR_WRONG_DATABASE=Unable to access data object
while validating user entered memory ranges. |
| PRESERVE_MEM_RANGE_MEM_NOT_SELECTED=You
have selected to preserve an area of memory but have not selected to
program that area. Please check the preserved ranges on the debug
tool's, "Memories to Program" property page, and make sure that any
preserved memory is also designated to be programmed. |
| PRESERVE_MEM_RANGE_OUT_OF_BOUNDS=The
selected preserve range, %s, does not fall within the proper range for
the memory area selected. Please check the manual program ranges on the
debug tool's, "Memories to Program" property page. |
| PRESERVE_MEM_RANGE_STRING_MALFORMED=The
preserve memory range(s) entered on the, "Memories to Program" property
page (%s) is not formatted properly. |
| PRESERVE_MEM_RANGE_WONT_BE_PROGRAMMED=Some
or all of the preserve memory ranges (%s) entered on the, "Memories to
Program" property page, do not fall under the indicated program range(s)
(%s) for the memory selected. Please check the preserved ranges on the
debug tool's, "Memories to Program" property page. |
| PROGRAM_COMPLETE=Programming/Verify
complete. |
| PROGRAM_MEMORY=program memory. |
| PROGRAM=program. |
| PROGRAMMING_DID_NOT_COMPLETE=Programming
did not complete. |
| READ_COMPLETE=Read complete. |
| READ_DID_NOT_COMPLETE=Read did not
complete. |
| RELEASEMCLR_FAILED=Release from reset
failed. |
| REMOVING_SWBPS_COMPLETE=Removing software
breakpoints complete. |
| REMOVING_SWBPS=Removing software
breakpoints... |
| RESET_FAILED=Failed to reset the
device. |
| RESETTING=Resetting... |
| RUN_INTERRUPT_THREAD_SYNCH_ERROR=An
internal run error has occurred. It is advised that you restart your
debug session. You may continue running but certain run time features
may no longer work properly. |
| RUN_TARGET_FAILED=Unable to run the target
device. |
| RUNNING=Running. |
| SD_RESULT_NO_ERROR=Empty Trace File
result |
| SERIAL_NUM=Serial Number:\n |
| SETTING_SWBPS=Setting software
breakpoints....... |
| STACK=stack. |
| START_AND_END_ADDR=start address = 0x%x,
end address = 0x%x. |
| START=start. |
| TARGET_DETECTED=Target voltage
detected. |
| TARGET_FOUND=Target device %s
found. |
| TARGET_HALTED=Target Halted. |
| TARGET_NOT_READY_4_DEBUG=The target device
is not ready for debugging. Please check your configuration bit settings
and program the device before proceeding. The most common causes for
this failure are oscillator and/or PGC/PGD settings. |
| TARGET_VDD=Target VDD: |
| TEST=test. |
| TOOL_IS_BUSY=ICE 4 is busy. Please wait for
the current operation to finish. |
| TOOL_VDD=VDD: |
| TOOL_VPP=VPP: |
| UNABLE_TO_OBTAIN_RESET_VECTOR=ICE 4 was
unable to retrieve the reset vector address. This indicates that no
_reset symbol has been defined and may prevent the device from starting
up properly. |
| UNKNOWN_MEMTYPE=Unknown memory
type. |
| UNLOAD_WHILE_BUSY=ICE 4 was unloaded while
still busy. Please unplug and reconnect the USB cable before using ICE 4
again. |
| UPDATING_APP=Updating firmware
application... |
| UPDATING_BOOTLOADER=Updating firmware
bootloader... |
| UPDATING_FPGA=Updating firmware
FPGA... |
| USE_LVP_PROGRAMMING=NOTE: If you would like
to program this device using low voltage programming, select Cancel on
this dialog. Then go to the ICE4 node of the project properties and
check the Enable Low Voltage Programming check box of the Program
Options Option Category pane (low voltage programming is not valid for
debugging operations). |
| USERID_MEMORY=User Id Memory. |
| USERID=user Id. |
| VERIFY_COMPLETE=Verification
successful. |
| VERIFY_FAILED=Verify failed. |
| VERSIONS=Versions. |
| VOLTAGES=Voltages. |
| WOULD_YOU_LIKE_TO_CONTINUE=Would you like
to continue? |