9.1 Emulator Selection and Switching
Use the Project Properties dialog to select or switch emulators for a project. To switch you must have more than one MPLAB® ICE 4 In-Circuit Emulator connected to your computer. MPLAB X IDE will differentiate between the two by displaying two different serial numbers.
To select or change the emulator used for a project:
- Open the Project Properties dialog by doing one of the following:
- Click on the project name in the Projects window and select File>Project Properties.
- Right click on the project name in the Projects window and select “Properties.”
- Under “Categories,” click on “Conf: [default].”
- Under “Hardware Tools,” find “ICE 4” and click on a serial number (SN) to select an emulator for use in the project.