3 CI/CD Hardware-in-the-Loop Example - 32-bit Target
The following example demonstrates how to perform CI/CD hardware-in-loop functionality using the MPLAB ICE 4 Breakout Board with the MPLAB ICE 4 in-circuit emulator and an 32-bit device target.
Important: Please see the CI/CD Wizard in MPLAB X IDE
User's Guide (DS-50003243), 1. CI/CD Wizard, “CI/CD Requirements” and
1.3 Getting Started with Jenkins, 1.3.1 “Prerequisites,” to determine what
licenses, along with general software and hardware will be required to use this example.
The user’s guide and additional information on CI/CD may be found on the MPLAB® X IDE CI/CD Wizard webpage.