1 Harmony 3 Driver and System Service Application Examples for SAMA5D2 Family

The following applications are provided to demonstrate the typical or interesting usage models of one or more drivers and system services.
NameDescription
FAT Filesystem throughput using SDMMC MediaThis application calculates throughput by Writing and Reading data into a SD-Card at High Speed using the MPLAB Harmony File System and the SDMMC driver
FAT Filesystem using SDMMC MediaThis application shows an example of using the MPLAB Harmony File System to access and modify the contents of a SD card using the SDMMC driver
FAT Filesystem using SQI Flash MediaThis application shows an example of using the MPLAB Harmony File System to access SQI based flash media. The SAMA5D29 Curiosity, SAMA5D27-SOM1-EK1 and the SAMA5D27-WLSOM1-EK1 has SST26 QSPI Flash
FreeRTOS BasicThis example application demonstrates context switching between four tasks of different priorities. Two tasks run periodically while the other two tasks are event driven
FreeRTOS Task NotificationThis example application is to illustrate the FreeRTOS Task Notification feature which is used as a light weight binary semaphore
I2C Driver Asynchronous - I2C EEPROMThis example application shows how to use the I2C driver in asynchronous mode to perform operations on the EEPROM
I2C Driver Synchronous - I2C EEPROMThis example application shows how to use the I2C driver in synchronous mode to perform operations on the EEPROM
I2C EEPROM AT24 Driver - EEPROM Read WriteThis example application shows how to use the AT24 driver to perform read and write operations on AT24 series of EEPROM
Memory Driver Asynchronous - SST26 QSPI Flash Read WriteThis example application shows how to use the Memory driver in asynchronous mode to perform block operations on the SST26 QSPI flash media
Memory Driver Synchronous - SST26 QSPI Flash Read WriteThis example application shows how to use the Memory driver in synchronous mode to perform block operations on the SST26 QSPI flash media
SDMMC driver asynchronous - SDIO Read Write

This example application shows how to use the SDMMC driver in

asynchronous mode to perform read/write operations using SDIO

interface on the SD Card Media

SDMMC Driver Asynchronous - SDMMC Read WriteThis example application shows how to use the SDMMC driver in asynchronous mode to perform block operations on the SD Card Media
SDSPI Driver Asynchronous - SDSPI Read WriteThis example application shows how to use the SDSPI driver in asynchronous mode to perform block operations on the SD Card Media
SDSPI Driver Synchronous - SDSPI Read WriteThis example application shows how to use the SDSPI driver in synchronous mode to perform block operations on the SD Card Media
SPI Driver Asynchronous - Multi ClientThis example demonstrates how to use single instance of the SPI driver in asynchronous mode to communicate with multiple EEPROMs
SPI Driver Asynchronous - Self Loopback Multi ClientThis example demonstrates how to use the SPI driver in asynchronous mode to achieve self-loop back between multiple clients
SPI Driver Synchronous - Multi ClientThis example demonstrates how to use single instance of the SPI driver in synchronous mode to communicate with multiple EEPROMs in an RTOS environment
SPI Driver Synchronous - Self Loopback Multi ClientThis example demonstrates how to use the SPI driver in synchronous mode to achieve self-loop back between multiple clients in RTOS environment
SPI EEPROM AT25 Driver - EEPROM Read WriteThis example application shows how to use the AT25 driver to perform read and write operations on AT25 series of EEPROM
SST26 SQI Flash Driver - Flash read write in SPI modeThis example application shows how to use the AT25DF SPI flash driver to perform block operations on the on-board SST26 Flash memory in SPI mode
SST26 SQI flash driver - Flash read write in SQI modeThis example application shows how to use the SST26 QSPI flash driver to perform block operations on the on-board SST26 QSPI Flash memory
Time System Service Multi-clientThis example application demonstrates the multi-client system timer functionality
USART Driver Asynchronous - USART EchoThis example echoes the received characters over the console using the USART driver in asynchronous mode
USART Driver Asynchronous - USART Multi InstanceThis example echoes the received characters over the two consoles using the USART driver in asynchronous mode
USART Driver Synchronous - USART EchoThis example echoes the received characters over the console using the USART driver in synchronous mode
USART Driver Synchronous - USART Multi InstanceThis example echoes the received characters over the two consoles using the USART driver in synchronous mode