8 Command-Line Utility
Microchip Studio comes with a command-line utility called atprogram that can be used to program targets using the STK600. During the Microchip Studio installation, a shortcut called “Microchip Studio 7.0 Command Prompt” was created in the Atmel folder on the Start menu. By double-clicking this shortcut, a command prompt will be opened, and programming commands can be entered. The command-line utility is installed in the Microchip Studio installation path in the folder Atmel/Studio/7.0/atbackend/.
For more help on the command-line utility, type the command:
atprogram --help