1.4.3.5 PAL_PLC_TxRequest Function
C
void PAL_PLC_TxRequest(PAL_PLC_HANDLE handle, uint8_t *pData, uint16_t length);
Summary
Allows a client to transmit data through PLC device.
Description
This routine sends a new data message through PLC using the PLC PAL module. The message must have a valid IEEE 802.15.4 MAC format with its corresponding MAC header.
Precondition
PAL_PLC_HandleGet must have been called to obtain a valid PLC PAL handle.
Parameters
| Param | Description |
|---|---|
| handle | A valid handle, returned from PAL_PLC_HandleGet |
| pData | Pointer to the data to transmit |
| length | Length of the data to transmit in bytes |
Returns
None.
Example
// 'palPlcHandle', returned from the PAL_PLC_HandleGet
MAC_RT_HEADER macHeader;
uint16_t totalLength;
uint16_t headerLength;
uint16_t payloadLength = 100;
uint8_t txData[MAC_RT_DATA_MAX_SIZE];
uint8_t payloadData[MAC_RT_MAX_PAYLOAD_SIZE];
// Local function implemented in the upper layer
headerLength = _buildMacHeader(txData, &macHeader);
memcpy(&txData[headerLength], payloadData, payloadLength);
totalLength = headerLength + payloadLength;
PAL_PLC_TxRequest(palPlcHandle, txData, totalLength);
Remarks
None.