1.4.3.15 PAL_PLC_DataIndication Typedef

C

typedef void (*PAL_PLC_DataIndication)(uint8_t *pData, uint16_t length);

Summary

Pointer to a PLC PAL Data Indication event handler function.

Description

This data type defines the required function signature for the PLC PAL reception data indication event handling callback function. When PAL_PLC_Initialize is called, a client must register a pointer whose function signature (parameter and return value types) matches the types specified by this function pointer in order to receive transfer related event calls back from the PLC PAL.

The parameters and return values are described here and a partial example implementation is provided.

Parameters

ParamDescription
pDataPointer to the data buffer containing received data
lengthLength of the received data in bytes

Returns

None.

Example

static void _plcDataIndication(uint8_t *pData, uint16_t length)
{
    // Reception handling here.
}

PAL_PLC_INIT palPlcInitData;
SYS_MODULE_OBJ palPlcObj;

palPlcInitData.macRtBand = G3_FCC;
palPlcInitData.macRtHandlers.palPlcDataIndication = _plcDataIndication;
palPlcInitData.macRtHandlers.palPlcTxConfirm = _plcTxConfirm;
palPlcInitData.macRtHandlers.palPlcCommStatusIndication = _plcCommStatusIndication;
palPlcInitData.macRtHandlers.palPlcRxParamsIndication = _plcRxParamsIndication;
palPlcInitData.initMIB = true;

// Initialize the PLC PAL module
palPlcObj = PAL_PLC_Initialize(PAL_PLC_PHY_INDEX, (const SYS_MODULE_INIT *) &palPlcInitData);

Remarks

None.