9.3.3 Preventing Flash/EEPROM Corruption
During periods of low VDD, the Flash program or EEPROM data can be corrupted if the supply voltage is too low for the CPU and the Flash/EEPROM to operate properly. These issues are the same on-board level systems using Flash/EEPROM, and the same design solutions may be applied.
A Flash/EEPROM corruption can be caused by two situations when the voltage is too low: 
      - A regular write sequence to the Flash, which requires a minimum voltage to operate correctly.
- The CPU itself can execute instructions incorrectly when the supply voltage is too low.
Attention: Flash/EEPROM corruption can be avoided by taking these measures:
   - Keep the device in Reset during periods of insufficient power supply voltage. This can be done by enabling the internal Brown-out Detector (BOD).
- The voltage level monitor in the BOD can be used to prevent starting a write to the EEPROM close to the BOD level.
- If the detection levels of the internal BOD do not match the required detection level, an external low VDD Reset protection circuit can be used. If a Reset occurs while a write operation is ongoing, the write operation will be aborted.