12.3 Project Introduction
This example uses the port pin change interrupt feature to monitor the PB7 level change. Every PB7 level change will trigger an interrupt to change the PB5 output according to the PB7 level status. The following is an example application firmware flow.