13.8 Scanning Modes
The interaction of the scanner with the system operation is controlled by the priority
            selection in the system arbiter (refer to the “Memory Access Scheme” section for
            more details). When using the scanner module in conjunction with the CRC module, the
            system arbiter needs to be configured such that the scanner has a higher priority than
            the CPU to ensure that a memory access request is granted when it occurs. Additionally,
                BURSTMD
            and TRIGEN
            bits also determine the operation of the scanner.