25.6.6.4 Suspend/Resume
This feature can be enabled by writing a ‘1’ to CTRLA.SUSPEN. Any modify operation, such as write/erase can be suspended even those triggered by the SmartEEPROM.
When enabled, the following commands are suspended by a NVM read request:
- EB
- WP
If a read occurs while executing one of the commands listed above, the NVMCTRL will follow these steps:
- Send a suspend command to the NVM.
- Wait for the NVM to be ready.
- Read the NVM. The NVMCTRL will persist in this step when a new read request occurs or else proceed.
- Resume the suspended operation.
A suspend operation will set INTFLAG.SUSP. To clear it, write a ‘1’ to INTFLAG.SUSP.
The NVM suspended state is reflected in STATUS.SUSP.
Limitations:
- Suspend is not possible for a read in the page being programmed.
- Suspend is not possible for a read in a sector (128 KB) containing a block under erase.
- It is not possible to enter power reduction mode when a command is suspended.