2 Silicon Errata Issues

The following errata issues apply to the PIC32MZ W1 family of devices.
Note:
  1. Cells with an X indicate the issue is present in this revision of the silicon.
  2. Cells with a dash (—) indicate the issue does not exist for this revision of the silicon.
  3. Blank cells indicate the issue is corrected or does not exist in this revision of the silicon.
Note: Traditional Inter-Integrated Circuit (I2C) and Serial Peripheral Interface (SPI) documentation uses the terminology “Master” and “Slave”. The equivalent Microchip terminology used in this document is “Host” and “Client”, respectively.