3.3.2 Using the Library

This topic describes the basic architecture of the USB Audio v1.0 Host Client Driver Library and provides information and examples on its use.

Topics

Name Description
Abstraction ModelDescribes the Abstraction Model of the USB Audio v1.0 Host Client Driver Library.
Library OverviewThe USB Audio v1.0 Host Client Driver can be grouped functionally as shown in the following table.
How the Library WorksDescribes how the library works and how it should be used.