3.4.2 Using the Library

Topics

Name Description
Abstraction ModelDescribes the Abstraction Model of the USB CDC Host Client Driver Library.
Library OverviewThe USB CDC Host Client Driver API is grouped functionally, as shown in the following table.
How the Library WorksDescribes how the Library works and how it should be used.