3.5.2 Using the Library

This topic describes the basic architecture of the USB HID Host Mouse Driver Library and provides information and examples on its use.

Topics

Name Description
Abstraction ModelDescribes the Abstraction Model of the USB HID Host Mouse Driver Library.
Library OverviewThe USB HID Host Mouse Driver can be grouped functionally as shown in the following table.
How the Library WorksDescribes how the library works and how it should be used.