4.2 Board Setup
Follow these steps before using the SAMA7G54 Curiosity Pro:
- Unpack the board, taking care to avoid electrostatic discharge.
- Verify the default jumper settings (see Default Jumper Settings).
- Connect to the PC as a power source:
- Use a USB Type-A-to-Type-C® cable to connect to connector J1 (USBA port).
- Connect the other end of the cable to an available port on the PC or a standard USB Type-A power source, such as a wall adapter.
- Connect a USB-UART converter to J63, ensuring that the VBUS_FTDI power source is also connected.
- Open a terminal on the PC for the USB-UART converter using the following settings: console 115200, N, 8, 1.
- Reset the board. The startup message “RomBOOT” appears on the console.