1.6.7 PIC32CM JH01 CURIOSITY Pro Onboard Sensor Example

Path of the application within the repository is apps/onboard_sensor/pic32cm_jh_cpro/

To build the application, refer to the following table and open the project using its IDE.

Hardware Setup

  1. Project uses PIC32CM JH01 Curiosity Pro Evaluation Kit
  2. Connect the Debug USB port on the board to the computer using a micro USB cable

Running The Application

  1. Open the application project pic32cm_jh_curiosity_pro.X in the IDE
  2. Build the project and program the target board

Monitoring Touch Data in MPLAB® DV Touch plugin

Prerequisite MPLAB® Data Visualizer and Touch Pluign. Procedure for Installation is available in Touch Plugin Installation.

  1. Configure COM Port
    • Select the correct COM port in Connection tab
    • Update the Baud Rate to 115200 in COM Settings
    • Start Streaming for COM data
  2. COM Port on Touch
    • Select Touch in Connection tab
    • For data source, from drop-down menu, select configured COM port as source
    • Start Streaming on Touch

Detailed procedure can be found in Visualize Touch Data Using MPLAB® Data Visualizer page.