The L2 cache controller is configured into four banks, each bank contains 512 sets of 16 ways and each way contains a 64 byte block. This subdivision into banks facilitates increased available bandwidth between CPU masters and the L2 cache as each bank has its own 128-bit TL-C (TileLink Cached) inner port. Hence, multiple requests to different banks may proceed in parallel.
The outer port of the L2 cache controller is a 128-bit TL-C port shared amongst all banks and connected to a DDR controller (see Figure 1). The overall organization of the L2 cache controller is shown in the following figure.