When a peripheral, library or other external component is selected from the Project Resources Area, its corresponding configuration GUI is displayed in the Composer Area. The Composer Area (Figure 1) is where peripherals and libraries are configured based on the application’s requirements.
The EUSART Easy Setup tab in the Composer Area allows configuring various EUSART parameters related to transmission and reception operations.
In addition to the Easy Setup tab in the module’s Composer, MCC also provides a Registers tab (Figure 2). The Registers tab provides direct access to configure the module’s registers and settings, providing unrestricted access to the configuration of the module.
Any module configuration done using the Easy Setup tab will be reflected in the values displayed in the Registers tab. Likewise, changes performed in the Registers tab reflecteds in the values in the Easy Setup tab.
For any pin which has been configured in the Pin Manager Table View, additional configuration of that pin can be done using the Pin Module View in the Composer Area. To display the Pin Module View, click on the Pin Module tab in the Project Resources Area (see Figure 3.)