The MPLAB Code Configurator can be installed in two ways: via the Microchip Plugins Update Center or from the Microchip website. The following chapters describe these procedures and also the MCC update process.
The MCC plugin can also be downloaded from the Microchip website by typing the address www.microchip.com/mcc in a web browser, selecting the Current
Download tab, and downloading the Current Version .zip
file.
See Figure 2-2.
.zip
file was extracted and select the MCC plugin.
It may have a .nbm
file extension.When an MCC version newer than the one installed is available, the MPLAB X IDE will display a notification in the bottom right corner of the IDE window. By clicking on it, the plugin update wizard is launched. In the wizard, click on the Install button, and the software will download and install the new MCC plugin version. See figure below.
Older MCC versions are available at the same www.microchip.com/mcc address, under the Archive Download tab.