Atmel Studio: Support for new devices in Atmel Studio can be added by using the Device Pack Manager, which is found under Tools → Device Pack Manager.
For offline installers, go to http://packs.download.atmel.com/. To install a package, double click on the installer file and follow the instructions. Any open Atmel Studio window will have to be closed for the installation to take effect.
IAR: Support for new devices in IAR Embedded Workbench can be added by installing the latest service package. The service package is available at My Pages on https://iar.com.