MPLAB X: Support for new devices in MPLAB X can be added by using the MPLAB Pack Manager, which is found under Tools → Packs.
For offline installers, go to https://packs.download.microchip.com/. To install a package, double click on the installer file and follow the instructions. Any open MPLAB X window will have to be closed for the installation to take effect.