Matching to a Given 50Ω Impedance

Figure 1 shows an example for matching to 50Ω, and the following figure is an example of the transformation using a different network.
Figure 1. Matching to 50Ω


The following list provides a guideline on the transformation process (assuming ideal conditions):

Note: Consider following the rules of admittance deployment if the impedance transformation is done in the Smith Chart (without a network analyzer). The following figure shows an example application circuit for a 50Ω matching network. The antenna already has the target impedance so that the complex impedance ZL can match to the target impedance.
Figure 2. Example Application Circuit for 50Ω Matching