The Flash memory can be divided into three sections: Bootloader Code (BOOT), Application Code (APPCODE), Application Data (APPDATA), each consisting in a variable number of Flash pages (512-bytes blocks):
For security reasons, it is not possible to write to the section of Flash the code is currently executing from. Code writing to the APPCODE section needs to be executing from the BOOT section, and code writing to the APPDATA section must be executing from either the BOOT section or the APPCODE section.
BOOTSIZE | CODESIZE | BOOT Section | APPCODE Section | APPDATA Section |
---|---|---|---|---|
0 | — | 0 to FLASHEND | — | — |
>0 | 0 | 0 to BOOTEND | BOOTEND to FLASHEND | — |
>0 | ≤BOOTSIZE | 0 to BOOTEND | — | BOOTEND to FLASHEND |
>0 | >BOOTSIZE | 0 to BOOTEND | BOOTEND to APPEND | APPEND to FLASHEND |
A good way of making sure these fuses are set up as expected on a device is to use the
FUSES
macro in the bootloader code project. It can be found in
fuse.h
, which is included by io.h
:
#include <avr/io.h> FUSES = { .OSCCFG = CLKSEL_OSCHF_gc, // High frequency oscillator selected .SYSCFG0 = CRCSRC_NOCRC_gc | RSTPINCFG_GPIO_gc, // No CRC enabled, RST pin in GPIO mode .SYSCFG1 = SUT_64MS_gc, // Start-up time 64 ms .BOOTSIZE = 0x02, // BOOT size = 0x02 * 512 bytes = 1024 bytes .CODESIZE = 0x00 // All remaining Flash used as App code };
0x00
and may cause an unwanted configuration.By including this macro in the project, the fuse settings are included in
compiled files. To write the fuse setting at the same time as the Flash, the
*.elf
file must be selected instead of the *.hex
file during device programming.
In Atmel Studio 7.0, another method is to use the Production File tab from the Device Programming.
In Atmel Studio 7.0, the fuses can also be configured using Device Programing (Ctrl +Shift + P) - Fuses, as shown in the figure below.