diag_sram_status_t

enum diag_sram_status_t

This enumeration contains return codes for SRAM diagnostics tests.

SRAM_OK

0 - indicates that SRAM test is successful

 
SRAM_ERROR

1 - indicates that SRAM test is unsuccessful

 
SRAM_GLOBAL_ERROR

2 - indicates that SRAM test is unsuccessful in the test variables' addresses

 
SRAM_ADDR_ERROR

3 - indicates that SRAM test addresses are invalid

 
SRAM_LENGTH_ERROR

4 - indicates that SRAM test length is invalid

 
SRAM_INVALID_REGION

5 - indicates that SRAM region is invalid as it is reserved for global variables