13 Reference Documentation
The following table provides the set of collateral documents to ease integration and device ramp.
| Document Title | Content |
|---|---|
| “ATWILC1000/ATWILC3000 – Wi-Fi® Link Controller Linux® User’s Guide” | This user’s guide describes how to run Wi-Fi on the ATWILC1000 SD card and to run Wi-Fi/BLE on the ATWILC3000 Shield board on the SAMA5D4 Xplained Ultra running with the Linux kernel 4.9. |
| “ATWILC1000/ATWILC3000 – ATWILC Devices Linux® Porting Guide” | This user’s guide describes how to port the ATWILC1000 and ATWILC3000 Linux drivers to another platform, and contains all the required modifications for driver porting. |
| “ATWILC1000/ATWILC3000 – Baremetal Wi-Fi®/BLE Link Controller Software Design Guide” | This design guide helps the user in integrating ATWILC1000/ATWILC3000 in the application using RTOS from Advanced Software Framework (ASF). |
| “ATWINC/ATWILC/ATSAMB/ ATBTLC – MCHPRT2 User’s Guide” | This document provides detailed information about the MCHPRT2 tool, which allows the user to configure, evaluate and test an RF system, based on the ATWILC3000 amongst other devices. |
| “ATWILC3000A/ATWILC3000-MR110xA Errata” | This document details the anomalies identified in the ATWILC3000 family of devices. |
| “ATWILC3000A Reference Design Package” (available in the ATWILC3000A Reference Design Package on ATWILC3000-IC webpage under Supporting Collateral) | This reference design package contains the design collateral (Schematics, Bill of Materials, PCB design source files, Gerber) of the module, evaluation boards and its associated boards for the ATWILC3000A, which should help a user to get started with their design. |
| “ATWILC3000A – Deriving Application Gain Table Application Note” (available as a part of the ATWILC3000A Reference Design Package on ATWILC3000-IC webpage) |
This application note describes the Wi-Fi and BLE gain table structure and procedure to derive the application gain table. This document provides further details on the steps to update the device with the gain table. |
Note: For a complete listing of development
support tools and documentation, visit www.microchip.com/wwwproducts/en/ATWILC3000 or refer to the customer support section on options
to the nearest Microchip field representative.