58.3 External Analog Reference Connections
The following schematic checklist is only necessary if the application is using many of the external analog references. If the internal references are used instead, the circuits in the following two figures are not necessary.
| Signal Name | Description | Recommended Pin Connection |
|---|---|---|
| VREFx | External reference VREFA/VREFB/VREFC | Capacitors(2): refer to REG_9(1) |
| AVSS | Ground | - |
Note:
- Refer to the “Power Supply Electrical Specifications” from the Electrical Characteristics chapter.
- Decoupling capacitors must be placed close to the device, low ESR capacitors must be used for better decoupling.