3.1.5 PAL_TimerIsRunning Function
C
bool PAL_TimerIsRunning(TimerId_t timer_id)
Summary
Gets the status of running timer
Description
Checks if the timer of requested timer identifier is running
Precondition
Timer should have been started before using this function
Parameters
Param | Description |
---|---|
timer_id | Timer identifier |
Returns
bool - true
- false otherwise.
Example
PAL_Status_t retVal = PAL_FAILURE; TimerId_t appTimer; bool IsTimerRunning = false; static void AppTimerCallback(void *paramCb) { //Toggle LED } //Get the Id for the sotware timer instance PAL_TimerGetId(&appTimer); if (PAL_SUCCESS == PAL_TimerStart(appTimer, 5000, TIMEOUT_RELATIVE, (void *)AppTimerCallback, NULL, CALLBACK_SINGLE)) { //Timer Started //ToggleLED } IsTimerRunning = PAL_TimerIsRunning(appTimer); if(IsTimerRunning) { //Timer is running }
Remarks
None