3.1.2 PAL_Init Function
C
PAL_Status_t PAL_Init(void)
Summary
Initialization of PAL
Description
This function initializes the timers array and initializes the PAL layer variables
Precondition
SYS_TIME_Initialize() should have been called before calling this function.
Parameters
None.
Returns
PAL_SUCCESS - if PAL initialization is successful
PAL_FAILURE - otherwise
Example
PAL_Status_t retVal = PAL_FAILURE;
retVal = PAL_Init();
if (PAL_SUCCESS =! retVal)
{
while(1);
}
Remarks
This routine is called by the PHY layer during initialization. So, user can directly uses PAL APIs.